ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS8962_BUF_CONFIG1_t Union Reference

#include <fxls8962.h>

Collaboration diagram for FXLS8962_BUF_CONFIG1_t:
Collaboration graph

Data Fields

struct {
   uint8_t   trg_orient: 1
 
   uint8_t   _reserved_: 1
 
   uint8_t   trg_sdcd_ot: 1
 
   uint8_t   trg_sdcd_wt: 1
 
   uint8_t   buf_gate: 1
 
   uint8_t   buf_mode: 2
 
   uint8_t   buf_type: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1006 of file fxls8962.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 1010 of file fxls8962.h.

◆ b

struct { ... } b

◆ buf_gate

uint8_t buf_gate

Definition at line 1015 of file fxls8962.h.

◆ buf_mode

uint8_t buf_mode

Definition at line 1017 of file fxls8962.h.

◆ buf_type

uint8_t buf_type

Definition at line 1019 of file fxls8962.h.

◆ trg_orient

uint8_t trg_orient

Definition at line 1008 of file fxls8962.h.

◆ trg_sdcd_ot

uint8_t trg_sdcd_ot

Definition at line 1011 of file fxls8962.h.

◆ trg_sdcd_wt

uint8_t trg_sdcd_wt

Definition at line 1013 of file fxls8962.h.

◆ w

uint8_t w

Definition at line 1022 of file fxls8962.h.


The documentation for this union was generated from the following file: