ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS8962_ORIENT_STATUS_t Union Reference

#include <fxls8962.h>

Collaboration diagram for FXLS8962_ORIENT_STATUS_t:
Collaboration graph

Data Fields

struct {
   uint8_t   bafro: 1
 
   uint8_t   lapo: 2
 
   uint8_t   _reserved_: 3
 
   uint8_t   lo: 1
 
   uint8_t   new_orient: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1118 of file fxls8962.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 1126 of file fxls8962.h.

◆ b

struct { ... } b

◆ bafro

uint8_t bafro

Definition at line 1122 of file fxls8962.h.

◆ lapo

uint8_t lapo

Definition at line 1124 of file fxls8962.h.

◆ lo

uint8_t lo

Definition at line 1127 of file fxls8962.h.

◆ new_orient

uint8_t new_orient

Definition at line 1129 of file fxls8962.h.

◆ w

uint8_t w

Definition at line 1132 of file fxls8962.h.


The documentation for this union was generated from the following file: