ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS8962_ORIENT_CONFIG_t Union Reference

#include <fxls8962.h>

Collaboration diagram for FXLS8962_ORIENT_CONFIG_t:
Collaboration graph

Data Fields

struct {
   uint8_t   _reserved_: 6
 
   uint8_t   orient_enable: 1
 
   uint8_t   orient_dbcntm: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1174 of file fxls8962.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 1178 of file fxls8962.h.

◆ b

struct { ... } b

◆ orient_dbcntm

uint8_t orient_dbcntm

Definition at line 1181 of file fxls8962.h.

◆ orient_enable

uint8_t orient_enable

Definition at line 1179 of file fxls8962.h.

◆ w

uint8_t w

Definition at line 1184 of file fxls8962.h.


The documentation for this union was generated from the following file: