ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS8962_ORIENT_BF_ZCOMP_t Union Reference

#include <fxls8962.h>

Collaboration diagram for FXLS8962_ORIENT_BF_ZCOMP_t:
Collaboration graph

Data Fields

struct {
   uint8_t   orient_zlock: 3
 
   uint8_t   _reserved_: 3
 
   uint8_t   orient_bkfr: 2
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1223 of file fxls8962.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 1229 of file fxls8962.h.

◆ b

struct { ... } b

◆ orient_bkfr

uint8_t orient_bkfr

Definition at line 1230 of file fxls8962.h.

◆ orient_zlock

uint8_t orient_zlock

Definition at line 1227 of file fxls8962.h.

◆ w

uint8_t w

Definition at line 1233 of file fxls8962.h.


The documentation for this union was generated from the following file: