ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS8962_SDCD_INT_SRC2_t Union Reference

#include <fxls8962.h>

Collaboration diagram for FXLS8962_SDCD_INT_SRC2_t:
Collaboration graph

Data Fields

struct {
   uint8_t   _reserved_: 1
 
   uint8_t   z_wt_ef: 1
 
   uint8_t   _reserved_1: 1
 
   uint8_t   y_wt_ef: 1
 
   uint8_t   _reserved_2: 1
 
   uint8_t   x_wt_ef: 1
 
   uint8_t   _reserved_3: 1
 
   uint8_t   wt_ea: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1424 of file fxls8962.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 1428 of file fxls8962.h.

◆ _reserved_1

uint8_t _reserved_1

Definition at line 1431 of file fxls8962.h.

◆ _reserved_2

uint8_t _reserved_2

Definition at line 1434 of file fxls8962.h.

◆ _reserved_3

uint8_t _reserved_3

Definition at line 1437 of file fxls8962.h.

◆ b

struct { ... } b

◆ w

uint8_t w

Definition at line 1441 of file fxls8962.h.

◆ wt_ea

uint8_t wt_ea

Definition at line 1438 of file fxls8962.h.

◆ x_wt_ef

uint8_t x_wt_ef

Definition at line 1435 of file fxls8962.h.

◆ y_wt_ef

uint8_t y_wt_ef

Definition at line 1432 of file fxls8962.h.

◆ z_wt_ef

uint8_t z_wt_ef

Definition at line 1429 of file fxls8962.h.


The documentation for this union was generated from the following file: