ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS8962_SDCD_CONFIG1_t Union Reference

#include <fxls8962.h>

Collaboration diagram for FXLS8962_SDCD_CONFIG1_t:
Collaboration graph

Data Fields

struct {
   uint8_t   z_wt_en: 1
 
   uint8_t   y_wt_en: 1
 
   uint8_t   x_wt_en: 1
 
   uint8_t   z_ot_en: 1
 
   uint8_t   y_ot_en: 1
 
   uint8_t   x_ot_en: 1
 
   uint8_t   wt_ele: 1
 
   uint8_t   ot_ele: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1484 of file fxls8962.h.

Field Documentation

◆ b

struct { ... } b

◆ ot_ele

uint8_t ot_ele

Definition at line 1502 of file fxls8962.h.

◆ w

uint8_t w

Definition at line 1505 of file fxls8962.h.

◆ wt_ele

uint8_t wt_ele

Definition at line 1500 of file fxls8962.h.

◆ x_ot_en

uint8_t x_ot_en

Definition at line 1498 of file fxls8962.h.

◆ x_wt_en

uint8_t x_wt_en

Definition at line 1492 of file fxls8962.h.

◆ y_ot_en

uint8_t y_ot_en

Definition at line 1496 of file fxls8962.h.

◆ y_wt_en

uint8_t y_wt_en

Definition at line 1490 of file fxls8962.h.

◆ z_ot_en

uint8_t z_ot_en

Definition at line 1494 of file fxls8962.h.

◆ z_wt_en

uint8_t z_wt_en

Definition at line 1488 of file fxls8962.h.


The documentation for this union was generated from the following file: