ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS8962_SDCD_CONFIG2_t Union Reference

#include <fxls8962.h>

Collaboration diagram for FXLS8962_SDCD_CONFIG2_t:
Collaboration graph

Data Fields

struct {
   uint8_t   ref_upd: 1
 
   uint8_t   mode: 1
 
   uint8_t   wt_log_sel: 1
 
   uint8_t   wt_dbctm: 1
 
   uint8_t   ot_dbctm: 1
 
   uint8_t   ref_updm: 2
 
   uint8_t   sdcd_en: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1578 of file fxls8962.h.

Field Documentation

◆ b

struct { ... } b

◆ mode

uint8_t mode

Definition at line 1584 of file fxls8962.h.

◆ ot_dbctm

uint8_t ot_dbctm

Definition at line 1590 of file fxls8962.h.

◆ ref_upd

uint8_t ref_upd

Definition at line 1582 of file fxls8962.h.

◆ ref_updm

uint8_t ref_updm

Definition at line 1592 of file fxls8962.h.

◆ sdcd_en

uint8_t sdcd_en

Definition at line 1594 of file fxls8962.h.

◆ w

uint8_t w

Definition at line 1597 of file fxls8962.h.

◆ wt_dbctm

uint8_t wt_dbctm

Definition at line 1588 of file fxls8962.h.

◆ wt_log_sel

uint8_t wt_log_sel

Definition at line 1586 of file fxls8962.h.


The documentation for this union was generated from the following file: