ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS8974_SYS_MODE_t Union Reference

#include <fxls8974.h>

Collaboration diagram for FXLS8974_SYS_MODE_t:
Collaboration graph

Data Fields

struct {
   uint8_t   sys_mode: 2
 
   uint8_t   buf_gate_cnt: 5
 
   uint8_t   buf_gate_error: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 353 of file fxls8974.h.

Field Documentation

◆ b

struct { ... } b

◆ buf_gate_cnt

uint8_t buf_gate_cnt

Definition at line 359 of file fxls8974.h.

◆ buf_gate_error

uint8_t buf_gate_error

Definition at line 361 of file fxls8974.h.

◆ sys_mode

uint8_t sys_mode

Definition at line 357 of file fxls8974.h.

◆ w

uint8_t w

Definition at line 364 of file fxls8974.h.


The documentation for this union was generated from the following file: