ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS8974_SENS_CONFIG4_t Union Reference

#include <fxls8974.h>

Collaboration diagram for FXLS8974_SENS_CONFIG4_t:
Collaboration graph

Data Fields

struct {
   uint8_t   int_pol: 1
 
   uint8_t   int_pp_od: 1
 
   uint8_t   int2_func: 1
 
   uint8_t   drdy_pul: 1
 
   uint8_t   wk_orient: 1
 
   uint8_t   wk_sdcd_ot: 1
 
   uint8_t   wk_sdcd_wt: 1
 
   uint8_t   ext_trig_m: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 591 of file fxls8974.h.

Field Documentation

◆ b

struct { ... } b

◆ drdy_pul

uint8_t drdy_pul

Definition at line 601 of file fxls8974.h.

◆ ext_trig_m

uint8_t ext_trig_m

Definition at line 609 of file fxls8974.h.

◆ int2_func

uint8_t int2_func

Definition at line 599 of file fxls8974.h.

◆ int_pol

uint8_t int_pol

Definition at line 595 of file fxls8974.h.

◆ int_pp_od

uint8_t int_pp_od

Definition at line 597 of file fxls8974.h.

◆ w

uint8_t w

Definition at line 612 of file fxls8974.h.

◆ wk_orient

uint8_t wk_orient

Definition at line 603 of file fxls8974.h.

◆ wk_sdcd_ot

uint8_t wk_sdcd_ot

Definition at line 605 of file fxls8974.h.

◆ wk_sdcd_wt

uint8_t wk_sdcd_wt

Definition at line 607 of file fxls8974.h.


The documentation for this union was generated from the following file: