ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS8974_BUF_CONFIG2_t Union Reference

#include <fxls8974.h>

Collaboration diagram for FXLS8974_BUF_CONFIG2_t:
Collaboration graph

Data Fields

struct {
   uint8_t   buf_wmrk: 6
 
   uint8_t   wake_src_buf: 1
 
   uint8_t   buf_flush: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1075 of file fxls8974.h.

Field Documentation

◆ b

struct { ... } b

◆ buf_flush

uint8_t buf_flush

Definition at line 1081 of file fxls8974.h.

◆ buf_wmrk

uint8_t buf_wmrk

Definition at line 1077 of file fxls8974.h.

◆ w

uint8_t w

Definition at line 1084 of file fxls8974.h.

◆ wake_src_buf

uint8_t wake_src_buf

Definition at line 1079 of file fxls8974.h.


The documentation for this union was generated from the following file: