ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS8974_ORIENT_THS_REG_t Union Reference

#include <fxls8974.h>

Collaboration diagram for FXLS8974_ORIENT_THS_REG_t:
Collaboration graph

Data Fields

struct {
   uint8_t   hys: 3
 
   uint8_t   orient_ths: 5
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1280 of file fxls8974.h.

Field Documentation

◆ b

struct { ... } b

◆ hys

uint8_t hys

Definition at line 1284 of file fxls8974.h.

◆ orient_ths

uint8_t orient_ths

Definition at line 1286 of file fxls8974.h.

◆ w

uint8_t w

Definition at line 1289 of file fxls8974.h.


The documentation for this union was generated from the following file: