ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_DR_STATUS_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_DR_STATUS_t:
Collaboration graph

Data Fields

struct {
   uint8_t   xdr: 1
 
   uint8_t   ydr: 1
 
   uint8_t   zdr: 1
 
   uint8_t   zyxdr: 1
 
   uint8_t   xow: 1
 
   uint8_t   yow: 1
 
   uint8_t   zow: 1
 
   uint8_t   zyxow: 1
 
} b
 
uint8_t w
 

Detailed Description

The following are the macro definitions to address each bit and its value in the hardware registers.

Definition at line 159 of file fxos8700.h.

Field Documentation

◆ b

struct { ... } b

◆ w

uint8_t w

Definition at line 170 of file fxos8700.h.

◆ xdr

uint8_t xdr

Definition at line 161 of file fxos8700.h.

◆ xow

uint8_t xow

Definition at line 165 of file fxos8700.h.

◆ ydr

uint8_t ydr

Definition at line 162 of file fxos8700.h.

◆ yow

uint8_t yow

Definition at line 166 of file fxos8700.h.

◆ zdr

uint8_t zdr

Definition at line 163 of file fxos8700.h.

◆ zow

uint8_t zow

Definition at line 167 of file fxos8700.h.

◆ zyxdr

uint8_t zyxdr

Definition at line 164 of file fxos8700.h.

◆ zyxow

uint8_t zyxow

Definition at line 168 of file fxos8700.h.


The documentation for this union was generated from the following file: