ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_OUT_Y_LSB_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_OUT_Y_LSB_t:
Collaboration graph

Data Fields

struct {
   uint8_t   _reserved_: 2
 
   uint8_t   yd: 6
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 353 of file fxos8700.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 355 of file fxos8700.h.

◆ b

struct { ... } b

◆ w

uint8_t w

Definition at line 359 of file fxos8700.h.

◆ yd

uint8_t yd

Definition at line 356 of file fxos8700.h.


The documentation for this union was generated from the following file: