ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_OUT_Z_MSB_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_OUT_Z_MSB_t:
Collaboration graph

Data Fields

struct {
   uint8_t   zd
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 380 of file fxos8700.h.

Field Documentation

◆ b

struct { ... } b

◆ w

uint8_t w

Definition at line 385 of file fxos8700.h.

◆ zd

uint8_t zd

Definition at line 382 of file fxos8700.h.


The documentation for this union was generated from the following file: