ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_TRIG_CFG_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_TRIG_CFG_t:
Collaboration graph

Data Fields

struct {
   uint8_t   _reserved_: 1
 
   uint8_t   trig_a_vecm: 1
 
   uint8_t   trig_a_ffmt: 1
 
   uint8_t   trig_pulse: 1
 
   uint8_t   trig_lndprt: 1
 
   uint8_t   trig_trans: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 473 of file fxos8700.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 475 of file fxos8700.h.

◆ b

struct { ... } b

◆ trig_a_ffmt

uint8_t trig_a_ffmt

Definition at line 477 of file fxos8700.h.

◆ trig_a_vecm

uint8_t trig_a_vecm

Definition at line 476 of file fxos8700.h.

◆ trig_lndprt

uint8_t trig_lndprt

Definition at line 479 of file fxos8700.h.

◆ trig_pulse

uint8_t trig_pulse

Definition at line 478 of file fxos8700.h.

◆ trig_trans

uint8_t trig_trans

Definition at line 480 of file fxos8700.h.

◆ w

uint8_t w

Definition at line 482 of file fxos8700.h.


The documentation for this union was generated from the following file: