ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_INT_SOURCE_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_INT_SOURCE_t:
Collaboration graph

Data Fields

struct {
   uint8_t   src_drdy: 1
 
   uint8_t   src_a_vecm: 1
 
   uint8_t   src_ffmt: 1
 
   uint8_t   src_pulse: 1
 
   uint8_t   src_lndprt: 1
 
   uint8_t   src_trans: 1
 
   uint8_t   src_fifo: 1
 
   uint8_t   src_aslp: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 570 of file fxos8700.h.

Field Documentation

◆ b

struct { ... } b

◆ src_a_vecm

uint8_t src_a_vecm

Definition at line 573 of file fxos8700.h.

◆ src_aslp

uint8_t src_aslp

Definition at line 579 of file fxos8700.h.

◆ src_drdy

uint8_t src_drdy

Definition at line 572 of file fxos8700.h.

◆ src_ffmt

uint8_t src_ffmt

Definition at line 574 of file fxos8700.h.

◆ src_fifo

uint8_t src_fifo

Definition at line 578 of file fxos8700.h.

◆ src_lndprt

uint8_t src_lndprt

Definition at line 576 of file fxos8700.h.

◆ src_pulse

uint8_t src_pulse

Definition at line 575 of file fxos8700.h.

◆ src_trans

uint8_t src_trans

Definition at line 577 of file fxos8700.h.

◆ w

uint8_t w

Definition at line 581 of file fxos8700.h.


The documentation for this union was generated from the following file: