ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_HP_FILTER_CUTOFF_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_HP_FILTER_CUTOFF_t:
Collaboration graph

Data Fields

struct {
   uint8_t   sel: 2
 
   uint8_t   _reserved_: 2
 
   uint8_t   pulse_lpf_en: 1
 
   uint8_t   pulse_hpf_byp: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 673 of file fxos8700.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 676 of file fxos8700.h.

◆ b

struct { ... } b

◆ pulse_hpf_byp

uint8_t pulse_hpf_byp

Definition at line 678 of file fxos8700.h.

◆ pulse_lpf_en

uint8_t pulse_lpf_en

Definition at line 677 of file fxos8700.h.

◆ sel

uint8_t sel

Definition at line 675 of file fxos8700.h.

◆ w

uint8_t w

Definition at line 680 of file fxos8700.h.


The documentation for this union was generated from the following file: