ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_PL_STATUS_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_PL_STATUS_t:
Collaboration graph

Data Fields

struct {
   uint8_t   bafro: 1
 
   uint8_t   lapo: 2
 
   uint8_t   _reserved_: 3
 
   uint8_t   lo: 1
 
   uint8_t   newlp: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 716 of file fxos8700.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 720 of file fxos8700.h.

◆ b

struct { ... } b

◆ bafro

uint8_t bafro

Definition at line 718 of file fxos8700.h.

◆ lapo

uint8_t lapo

Definition at line 719 of file fxos8700.h.

◆ lo

uint8_t lo

Definition at line 721 of file fxos8700.h.

◆ newlp

uint8_t newlp

Definition at line 722 of file fxos8700.h.

◆ w

uint8_t w

Definition at line 724 of file fxos8700.h.


The documentation for this union was generated from the following file: