ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_PL_THS_REG_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_PL_THS_REG_t:
Collaboration graph

Data Fields

struct {
   uint8_t   hys: 3
 
   uint8_t   pl_ths: 5
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 863 of file fxos8700.h.

Field Documentation

◆ b

struct { ... } b

◆ hys

uint8_t hys

Definition at line 865 of file fxos8700.h.

◆ pl_ths

uint8_t pl_ths

Definition at line 866 of file fxos8700.h.

◆ w

uint8_t w

Definition at line 868 of file fxos8700.h.


The documentation for this union was generated from the following file: