ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_A_FFMT_CFG_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_A_FFMT_CFG_t:
Collaboration graph

Data Fields

struct {
   uint8_t   _reserved_: 3
 
   uint8_t   xefe: 1
 
   uint8_t   yefe: 1
 
   uint8_t   zefe: 1
 
   uint8_t   oae: 1
 
   uint8_t   ele: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 913 of file fxos8700.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 915 of file fxos8700.h.

◆ b

struct { ... } b

◆ ele

uint8_t ele

Definition at line 920 of file fxos8700.h.

◆ oae

uint8_t oae

Definition at line 919 of file fxos8700.h.

◆ w

uint8_t w

Definition at line 922 of file fxos8700.h.

◆ xefe

uint8_t xefe

Definition at line 916 of file fxos8700.h.

◆ yefe

uint8_t yefe

Definition at line 917 of file fxos8700.h.

◆ zefe

uint8_t zefe

Definition at line 918 of file fxos8700.h.


The documentation for this union was generated from the following file: