ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_A_FFMT_SRC_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_A_FFMT_SRC_t:
Collaboration graph

Data Fields

struct {
   uint8_t   xhp: 1
 
   uint8_t   xhe: 1
 
   uint8_t   yhp: 1
 
   uint8_t   yhe: 1
 
   uint8_t   zhp: 1
 
   uint8_t   zhe: 1
 
   uint8_t   _reserved_: 1
 
   uint8_t   ea: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 971 of file fxos8700.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 979 of file fxos8700.h.

◆ b

struct { ... } b

◆ ea

uint8_t ea

Definition at line 980 of file fxos8700.h.

◆ w

uint8_t w

Definition at line 982 of file fxos8700.h.

◆ xhe

uint8_t xhe

Definition at line 974 of file fxos8700.h.

◆ xhp

uint8_t xhp

Definition at line 973 of file fxos8700.h.

◆ yhe

uint8_t yhe

Definition at line 976 of file fxos8700.h.

◆ yhp

uint8_t yhp

Definition at line 975 of file fxos8700.h.

◆ zhe

uint8_t zhe

Definition at line 978 of file fxos8700.h.

◆ zhp

uint8_t zhp

Definition at line 977 of file fxos8700.h.


The documentation for this union was generated from the following file: