ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_TRANSIENT_CFG_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_TRANSIENT_CFG_t:
Collaboration graph

Data Fields

struct {
   uint8_t   hpf_byp: 1
 
   uint8_t   xtefe: 1
 
   uint8_t   ytefe: 1
 
   uint8_t   ztefe: 1
 
   uint8_t   tele: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1061 of file fxos8700.h.

Field Documentation

◆ b

struct { ... } b

◆ hpf_byp

uint8_t hpf_byp

Definition at line 1063 of file fxos8700.h.

◆ tele

uint8_t tele

Definition at line 1067 of file fxos8700.h.

◆ w

uint8_t w

Definition at line 1069 of file fxos8700.h.

◆ xtefe

uint8_t xtefe

Definition at line 1064 of file fxos8700.h.

◆ ytefe

uint8_t ytefe

Definition at line 1065 of file fxos8700.h.

◆ ztefe

uint8_t ztefe

Definition at line 1066 of file fxos8700.h.


The documentation for this union was generated from the following file: