ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_TRANSIENT_SRC_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_TRANSIENT_SRC_t:
Collaboration graph

Data Fields

struct {
   uint8_t   trans_xpol: 1
 
   uint8_t   tran_xef: 1
 
   uint8_t   tran_ypol: 1
 
   uint8_t   tran_yef: 1
 
   uint8_t   tran_zpol: 1
 
   uint8_t   tran_zef: 1
 
   uint8_t   tran_ea: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1129 of file fxos8700.h.

Field Documentation

◆ b

struct { ... } b

◆ tran_ea

uint8_t tran_ea

Definition at line 1137 of file fxos8700.h.

◆ tran_xef

uint8_t tran_xef

Definition at line 1132 of file fxos8700.h.

◆ tran_yef

uint8_t tran_yef

Definition at line 1134 of file fxos8700.h.

◆ tran_ypol

uint8_t tran_ypol

Definition at line 1133 of file fxos8700.h.

◆ tran_zef

uint8_t tran_zef

Definition at line 1136 of file fxos8700.h.

◆ tran_zpol

uint8_t tran_zpol

Definition at line 1135 of file fxos8700.h.

◆ trans_xpol

uint8_t trans_xpol

Definition at line 1131 of file fxos8700.h.

◆ w

uint8_t w

Definition at line 1139 of file fxos8700.h.


The documentation for this union was generated from the following file: