ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_PULSE_CFG_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_PULSE_CFG_t:
Collaboration graph

Data Fields

struct {
   uint8_t   pls_xspefe: 1
 
   uint8_t   pls_xdpefe: 1
 
   uint8_t   pls_yspefe: 1
 
   uint8_t   pls_ydpefe: 1
 
   uint8_t   pls_zspefe: 1
 
   uint8_t   pls_zdpefe: 1
 
   uint8_t   pls_ele: 1
 
   uint8_t   pls_dpa: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1228 of file fxos8700.h.

Field Documentation

◆ b

struct { ... } b

◆ pls_dpa

uint8_t pls_dpa

Definition at line 1237 of file fxos8700.h.

◆ pls_ele

uint8_t pls_ele

Definition at line 1236 of file fxos8700.h.

◆ pls_xdpefe

uint8_t pls_xdpefe

Definition at line 1231 of file fxos8700.h.

◆ pls_xspefe

uint8_t pls_xspefe

Definition at line 1230 of file fxos8700.h.

◆ pls_ydpefe

uint8_t pls_ydpefe

Definition at line 1233 of file fxos8700.h.

◆ pls_yspefe

uint8_t pls_yspefe

Definition at line 1232 of file fxos8700.h.

◆ pls_zdpefe

uint8_t pls_zdpefe

Definition at line 1235 of file fxos8700.h.

◆ pls_zspefe

uint8_t pls_zspefe

Definition at line 1234 of file fxos8700.h.

◆ w

uint8_t w

Definition at line 1239 of file fxos8700.h.


The documentation for this union was generated from the following file: