ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_PULSE_SRC_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_PULSE_SRC_t:
Collaboration graph

Data Fields

struct {
   uint8_t   pls_src_polx: 1
 
   uint8_t   pls_src_poly: 1
 
   uint8_t   pls_src_polz: 1
 
   uint8_t   pls_src_dpe: 1
 
   uint8_t   pls_src_axx: 1
 
   uint8_t   pls_src_axy: 1
 
   uint8_t   pls_src_axz: 1
 
   uint8_t   pls_src_ea: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1313 of file fxos8700.h.

Field Documentation

◆ b

struct { ... } b

◆ pls_src_axx

uint8_t pls_src_axx

Definition at line 1319 of file fxos8700.h.

◆ pls_src_axy

uint8_t pls_src_axy

Definition at line 1320 of file fxos8700.h.

◆ pls_src_axz

uint8_t pls_src_axz

Definition at line 1321 of file fxos8700.h.

◆ pls_src_dpe

uint8_t pls_src_dpe

Definition at line 1318 of file fxos8700.h.

◆ pls_src_ea

uint8_t pls_src_ea

Definition at line 1322 of file fxos8700.h.

◆ pls_src_polx

uint8_t pls_src_polx

Definition at line 1315 of file fxos8700.h.

◆ pls_src_poly

uint8_t pls_src_poly

Definition at line 1316 of file fxos8700.h.

◆ pls_src_polz

uint8_t pls_src_polz

Definition at line 1317 of file fxos8700.h.

◆ w

uint8_t w

Definition at line 1324 of file fxos8700.h.


The documentation for this union was generated from the following file: