ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_CTRL_REG1_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_CTRL_REG1_t:
Collaboration graph

Data Fields

struct {
   uint8_t   active: 1
 
   uint8_t   f_read: 1
 
   uint8_t   lnoise: 1
 
   uint8_t   dr: 3
 
   uint8_t   aslp_rate: 2
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1480 of file fxos8700.h.

Field Documentation

◆ active

uint8_t active

Definition at line 1482 of file fxos8700.h.

◆ aslp_rate

uint8_t aslp_rate

Definition at line 1486 of file fxos8700.h.

◆ b

struct { ... } b

◆ dr

uint8_t dr

Definition at line 1485 of file fxos8700.h.

◆ f_read

uint8_t f_read

Definition at line 1483 of file fxos8700.h.

◆ lnoise

uint8_t lnoise

Definition at line 1484 of file fxos8700.h.

◆ w

uint8_t w

Definition at line 1488 of file fxos8700.h.


The documentation for this union was generated from the following file: