ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_CTRL_REG3_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_CTRL_REG3_t:
Collaboration graph

Data Fields

struct {
   uint8_t   pp_od: 1
 
   uint8_t   ipol: 1
 
   uint8_t   wake_a_vecm: 1
 
   uint8_t   wake_ffmt: 1
 
   uint8_t   wake_pulse: 1
 
   uint8_t   wake_lndprt: 1
 
   uint8_t   wake_trans: 1
 
   uint8_t   fifo_gate: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1611 of file fxos8700.h.

Field Documentation

◆ b

struct { ... } b

◆ fifo_gate

uint8_t fifo_gate

Definition at line 1620 of file fxos8700.h.

◆ ipol

uint8_t ipol

Definition at line 1614 of file fxos8700.h.

◆ pp_od

uint8_t pp_od

Definition at line 1613 of file fxos8700.h.

◆ w

uint8_t w

Definition at line 1622 of file fxos8700.h.

◆ wake_a_vecm

uint8_t wake_a_vecm

Definition at line 1615 of file fxos8700.h.

◆ wake_ffmt

uint8_t wake_ffmt

Definition at line 1616 of file fxos8700.h.

◆ wake_lndprt

uint8_t wake_lndprt

Definition at line 1618 of file fxos8700.h.

◆ wake_pulse

uint8_t wake_pulse

Definition at line 1617 of file fxos8700.h.

◆ wake_trans

uint8_t wake_trans

Definition at line 1619 of file fxos8700.h.


The documentation for this union was generated from the following file: