ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_CTRL_REG4_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_CTRL_REG4_t:
Collaboration graph

Data Fields

struct {
   uint8_t   int_en_drdy: 1
 
   uint8_t   int_en_a_vecm: 1
 
   uint8_t   int_en_ffmt: 1
 
   uint8_t   int_en_pulse: 1
 
   uint8_t   int_en_lndprt: 1
 
   uint8_t   int_en_trans: 1
 
   uint8_t   int_en_fifo: 1
 
   uint8_t   int_en_aslp: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1693 of file fxos8700.h.

Field Documentation

◆ b

struct { ... } b

◆ int_en_a_vecm

uint8_t int_en_a_vecm

Definition at line 1696 of file fxos8700.h.

◆ int_en_aslp

uint8_t int_en_aslp

Definition at line 1702 of file fxos8700.h.

◆ int_en_drdy

uint8_t int_en_drdy

Definition at line 1695 of file fxos8700.h.

◆ int_en_ffmt

uint8_t int_en_ffmt

Definition at line 1697 of file fxos8700.h.

◆ int_en_fifo

uint8_t int_en_fifo

Definition at line 1701 of file fxos8700.h.

◆ int_en_lndprt

uint8_t int_en_lndprt

Definition at line 1699 of file fxos8700.h.

◆ int_en_pulse

uint8_t int_en_pulse

Definition at line 1698 of file fxos8700.h.

◆ int_en_trans

uint8_t int_en_trans

Definition at line 1700 of file fxos8700.h.

◆ w

uint8_t w

Definition at line 1704 of file fxos8700.h.


The documentation for this union was generated from the following file: