ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_CTRL_REG5_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_CTRL_REG5_t:
Collaboration graph

Data Fields

struct {
   uint8_t   int_cfg_drdy: 1
 
   uint8_t   int_cfg_a_vecm: 1
 
   uint8_t   int_cfg_ffmt: 1
 
   uint8_t   int_cfg_pulse: 1
 
   uint8_t   int_cfg_lndprt: 1
 
   uint8_t   int_cfg_trans: 1
 
   uint8_t   int_cfg_fifo: 1
 
   uint8_t   int_cfg_aslp: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1766 of file fxos8700.h.

Field Documentation

◆ b

struct { ... } b

◆ int_cfg_a_vecm

uint8_t int_cfg_a_vecm

Definition at line 1769 of file fxos8700.h.

◆ int_cfg_aslp

uint8_t int_cfg_aslp

Definition at line 1775 of file fxos8700.h.

◆ int_cfg_drdy

uint8_t int_cfg_drdy

Definition at line 1768 of file fxos8700.h.

◆ int_cfg_ffmt

uint8_t int_cfg_ffmt

Definition at line 1770 of file fxos8700.h.

◆ int_cfg_fifo

uint8_t int_cfg_fifo

Definition at line 1774 of file fxos8700.h.

◆ int_cfg_lndprt

uint8_t int_cfg_lndprt

Definition at line 1772 of file fxos8700.h.

◆ int_cfg_pulse

uint8_t int_cfg_pulse

Definition at line 1771 of file fxos8700.h.

◆ int_cfg_trans

uint8_t int_cfg_trans

Definition at line 1773 of file fxos8700.h.

◆ w

uint8_t w

Definition at line 1777 of file fxos8700.h.


The documentation for this union was generated from the following file: