ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_M_OFF_Y_LSB_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_M_OFF_Y_LSB_t:
Collaboration graph

Data Fields

struct {
   uint8_t   _reserved_: 1
 
   uint8_t   m_off_y: 7
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 2120 of file fxos8700.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 2122 of file fxos8700.h.

◆ b

struct { ... } b

◆ m_off_y

uint8_t m_off_y

Definition at line 2123 of file fxos8700.h.

◆ w

uint8_t w

Definition at line 2125 of file fxos8700.h.


The documentation for this union was generated from the following file: