ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_TEMP_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_TEMP_t:
Collaboration graph

Data Fields

struct {
   uint8_t   die_temperature
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 2290 of file fxos8700.h.

Field Documentation

◆ b

struct { ... } b

◆ die_temperature

uint8_t die_temperature

Definition at line 2292 of file fxos8700.h.

◆ w

uint8_t w

Definition at line 2294 of file fxos8700.h.


The documentation for this union was generated from the following file: