ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_M_THS_CFG_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_M_THS_CFG_t:
Collaboration graph

Data Fields

struct {
   uint8_t   m_ths_int_cfg: 1
 
   uint8_t   m_ths_int_en: 1
 
   uint8_t   m_ths_wake_en: 1
 
   uint8_t   m_ths_xefe: 1
 
   uint8_t   m_ths_yefe: 1
 
   uint8_t   m_ths_zefe: 1
 
   uint8_t   m_ths_oae: 1
 
   uint8_t   m_ths_ele: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 2315 of file fxos8700.h.

Field Documentation

◆ b

struct { ... } b

◆ m_ths_ele

uint8_t m_ths_ele

Definition at line 2324 of file fxos8700.h.

◆ m_ths_int_cfg

uint8_t m_ths_int_cfg

Definition at line 2317 of file fxos8700.h.

◆ m_ths_int_en

uint8_t m_ths_int_en

Definition at line 2318 of file fxos8700.h.

◆ m_ths_oae

uint8_t m_ths_oae

Definition at line 2323 of file fxos8700.h.

◆ m_ths_wake_en

uint8_t m_ths_wake_en

Definition at line 2319 of file fxos8700.h.

◆ m_ths_xefe

uint8_t m_ths_xefe

Definition at line 2320 of file fxos8700.h.

◆ m_ths_yefe

uint8_t m_ths_yefe

Definition at line 2321 of file fxos8700.h.

◆ m_ths_zefe

uint8_t m_ths_zefe

Definition at line 2322 of file fxos8700.h.

◆ w

uint8_t w

Definition at line 2326 of file fxos8700.h.


The documentation for this union was generated from the following file: