ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_M_THS_SRC_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_M_THS_SRC_t:
Collaboration graph

Data Fields

struct {
   uint8_t   m_ths_xhp: 1
 
   uint8_t   m_ths_xhe: 1
 
   uint8_t   m_ths_yhp: 1
 
   uint8_t   m_ths_yhe: 1
 
   uint8_t   m_ths_zhp: 1
 
   uint8_t   m_ths_zhe: 1
 
   uint8_t   _reserved_: 1
 
   uint8_t   m_ths_ea: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 2368 of file fxos8700.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 2376 of file fxos8700.h.

◆ b

struct { ... } b

◆ m_ths_ea

uint8_t m_ths_ea

Definition at line 2377 of file fxos8700.h.

◆ m_ths_xhe

uint8_t m_ths_xhe

Definition at line 2371 of file fxos8700.h.

◆ m_ths_xhp

uint8_t m_ths_xhp

Definition at line 2370 of file fxos8700.h.

◆ m_ths_yhe

uint8_t m_ths_yhe

Definition at line 2373 of file fxos8700.h.

◆ m_ths_yhp

uint8_t m_ths_yhp

Definition at line 2372 of file fxos8700.h.

◆ m_ths_zhe

uint8_t m_ths_zhe

Definition at line 2375 of file fxos8700.h.

◆ m_ths_zhp

uint8_t m_ths_zhp

Definition at line 2374 of file fxos8700.h.

◆ w

uint8_t w

Definition at line 2379 of file fxos8700.h.


The documentation for this union was generated from the following file: