ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_M_CTRL_REG1_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_M_CTRL_REG1_t:
Collaboration graph

Data Fields

struct {
   uint8_t   m_hms: 2
 
   uint8_t   m_os: 3
 
   uint8_t   m_ost: 1
 
   uint8_t   m_rst: 1
 
   uint8_t   m_acal: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 2530 of file fxos8700.h.

Field Documentation

◆ b

struct { ... } b

◆ m_acal

uint8_t m_acal

Definition at line 2538 of file fxos8700.h.

◆ m_hms

uint8_t m_hms

Definition at line 2532 of file fxos8700.h.

◆ m_os

uint8_t m_os

Definition at line 2533 of file fxos8700.h.

◆ m_ost

uint8_t m_ost

Definition at line 2535 of file fxos8700.h.

◆ m_rst

uint8_t m_rst

Definition at line 2537 of file fxos8700.h.

◆ w

uint8_t w

Definition at line 2540 of file fxos8700.h.


The documentation for this union was generated from the following file: