ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_M_CTRL_REG2_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_M_CTRL_REG2_t:
Collaboration graph

Data Fields

struct {
   uint8_t   m_rst_cnt: 2
 
   uint8_t   m_maxmin_rst: 1
 
   uint8_t   m_maxmin_dis_ths: 1
 
   uint8_t   m_maxmin_dis: 1
 
   uint8_t   m_autoinc: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 2607 of file fxos8700.h.

Field Documentation

◆ b

struct { ... } b

◆ m_autoinc

uint8_t m_autoinc

Definition at line 2613 of file fxos8700.h.

◆ m_maxmin_dis

uint8_t m_maxmin_dis

Definition at line 2612 of file fxos8700.h.

◆ m_maxmin_dis_ths

uint8_t m_maxmin_dis_ths

Definition at line 2611 of file fxos8700.h.

◆ m_maxmin_rst

uint8_t m_maxmin_rst

Definition at line 2610 of file fxos8700.h.

◆ m_rst_cnt

uint8_t m_rst_cnt

Definition at line 2609 of file fxos8700.h.

◆ w

uint8_t w

Definition at line 2615 of file fxos8700.h.


The documentation for this union was generated from the following file: