ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_M_CTRL_REG3_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_M_CTRL_REG3_t:
Collaboration graph

Data Fields

struct {
   uint8_t   m_st_xy: 2
 
   uint8_t   m_st_z: 1
 
   uint8_t   m_ths_xyz_update: 1
 
   uint8_t   m_aslp_os: 3
 
   uint8_t   m_raw: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 2682 of file fxos8700.h.

Field Documentation

◆ b

struct { ... } b

◆ m_aslp_os

uint8_t m_aslp_os

Definition at line 2687 of file fxos8700.h.

◆ m_raw

uint8_t m_raw

Definition at line 2688 of file fxos8700.h.

◆ m_st_xy

uint8_t m_st_xy

Definition at line 2684 of file fxos8700.h.

◆ m_st_z

uint8_t m_st_z

Definition at line 2685 of file fxos8700.h.

◆ m_ths_xyz_update

uint8_t m_ths_xyz_update

Definition at line 2686 of file fxos8700.h.

◆ w

uint8_t w

Definition at line 2690 of file fxos8700.h.


The documentation for this union was generated from the following file: