ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_M_INT_SRC_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_M_INT_SRC_t:
Collaboration graph

Data Fields

struct {
   uint8_t   src_m_drdy: 1
 
   uint8_t   src_m_vecm: 1
 
   uint8_t   src_m_ths: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 2743 of file fxos8700.h.

Field Documentation

◆ b

struct { ... } b

◆ src_m_drdy

uint8_t src_m_drdy

Definition at line 2745 of file fxos8700.h.

◆ src_m_ths

uint8_t src_m_ths

Definition at line 2747 of file fxos8700.h.

◆ src_m_vecm

uint8_t src_m_vecm

Definition at line 2746 of file fxos8700.h.

◆ w

uint8_t w

Definition at line 2749 of file fxos8700.h.


The documentation for this union was generated from the following file: