ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_A_VECM_CFG_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_A_VECM_CFG_t:
Collaboration graph

Data Fields

struct {
   uint8_t   _reserved_: 4
 
   uint8_t   a_vecm_updm: 1
 
   uint8_t   a_vecm_initm: 1
 
   uint8_t   a_vecm_ele: 1
 
   uint8_t   a_vecm_en: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 2776 of file fxos8700.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 2778 of file fxos8700.h.

◆ a_vecm_ele

uint8_t a_vecm_ele

Definition at line 2781 of file fxos8700.h.

◆ a_vecm_en

uint8_t a_vecm_en

Definition at line 2782 of file fxos8700.h.

◆ a_vecm_initm

uint8_t a_vecm_initm

Definition at line 2780 of file fxos8700.h.

◆ a_vecm_updm

uint8_t a_vecm_updm

Definition at line 2779 of file fxos8700.h.

◆ b

struct { ... } b

◆ w

uint8_t w

Definition at line 2784 of file fxos8700.h.


The documentation for this union was generated from the following file: