ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_A_VECM_THS_MSB_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_A_VECM_THS_MSB_t:
Collaboration graph

Data Fields

struct {
   uint8_t   a_vbecm_ths: 5
 
   uint8_t   _reserved_: 2
 
   uint8_t   a_vbecm_dbcntm: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 2814 of file fxos8700.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 2817 of file fxos8700.h.

◆ a_vbecm_dbcntm

uint8_t a_vbecm_dbcntm

Definition at line 2818 of file fxos8700.h.

◆ a_vbecm_ths

uint8_t a_vbecm_ths

Definition at line 2816 of file fxos8700.h.

◆ b

struct { ... } b

◆ w

uint8_t w

Definition at line 2820 of file fxos8700.h.


The documentation for this union was generated from the following file: