ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXOS8700_M_VECM_CFG_t Union Reference

#include <fxos8700.h>

Collaboration diagram for FXOS8700_M_VECM_CFG_t:
Collaboration graph

Data Fields

struct {
   uint8_t   m_vecm_init_cfg: 1
 
   uint8_t   m_vecm_int_en: 1
 
   uint8_t   m_vecm_wake_en: 1
 
   uint8_t   a_vecm_en: 1
 
   uint8_t   m_vecm_updm: 1
 
   uint8_t   m_vecm_initm: 1
 
   uint8_t   m_vecm_ele: 1
 
   uint8_t   reserved: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 2965 of file fxos8700.h.

Field Documentation

◆ a_vecm_en

uint8_t a_vecm_en

Definition at line 2970 of file fxos8700.h.

◆ b

struct { ... } b

◆ m_vecm_ele

uint8_t m_vecm_ele

Definition at line 2973 of file fxos8700.h.

◆ m_vecm_init_cfg

uint8_t m_vecm_init_cfg

Definition at line 2967 of file fxos8700.h.

◆ m_vecm_initm

uint8_t m_vecm_initm

Definition at line 2972 of file fxos8700.h.

◆ m_vecm_int_en

uint8_t m_vecm_int_en

Definition at line 2968 of file fxos8700.h.

◆ m_vecm_updm

uint8_t m_vecm_updm

Definition at line 2971 of file fxos8700.h.

◆ m_vecm_wake_en

uint8_t m_vecm_wake_en

Definition at line 2969 of file fxos8700.h.

◆ reserved

uint8_t reserved

Definition at line 2974 of file fxos8700.h.

◆ w

uint8_t w

Definition at line 2976 of file fxos8700.h.


The documentation for this union was generated from the following file: