![]()  | 
  
    ISSDK
    1.8
    
   IoT Sensing Software Development Kit 
   | 
 
This structure holds information to receive a packet of data to the host. More...
#include <host_io_uart.h>

Data Fields | |
| uint8_t | rxState | 
| uint8_t | mIndex | 
| uint8_t * | pRxbuf | 
This structure holds information to receive a packet of data to the host.
Definition at line 49 of file host_io_uart.h.
| uint8_t mIndex | 
Definition at line 52 of file host_io_uart.h.
Referenced by HDLC_Process_Rx_Byte(), and Host_IO_Receive().
| uint8_t* pRxbuf | 
Definition at line 53 of file host_io_uart.h.
Referenced by HDLC_Process_Rx_Byte().
| uint8_t rxState | 
Definition at line 51 of file host_io_uart.h.
Referenced by HDLC_Process_Rx_Byte().