ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
ISL29023_CMD_I_t Union Reference

#include <isl29023.h>

Collaboration diagram for ISL29023_CMD_I_t:
Collaboration graph

Data Fields

struct {
   uint8_t   prst: 2
 
   uint8_t   flag: 1
 
   uint8_t   _reserved_: 2
 
   uint8_t   op: 3
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 35 of file isl29023.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 41 of file isl29023.h.

◆ b

struct { ... } b

◆ flag

uint8_t flag

Definition at line 39 of file isl29023.h.

◆ op

uint8_t op

Definition at line 42 of file isl29023.h.

◆ prst

uint8_t prst

Definition at line 37 of file isl29023.h.

◆ w

uint8_t w

Definition at line 45 of file isl29023.h.


The documentation for this union was generated from the following file: