ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
ISL29023_CMD_II_t Union Reference

#include <isl29023.h>

Collaboration diagram for ISL29023_CMD_II_t:
Collaboration graph

Data Fields

struct {
   uint8_t   range: 2
 
   uint8_t   res: 2
 
   uint8_t   _reserved_: 4
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 87 of file isl29023.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 93 of file isl29023.h.

◆ b

struct { ... } b

◆ range

uint8_t range

Definition at line 89 of file isl29023.h.

◆ res

uint8_t res

Definition at line 91 of file isl29023.h.

◆ w

uint8_t w

Definition at line 96 of file isl29023.h.


The documentation for this union was generated from the following file: