ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
MAG3110_DR_STATUS_t Union Reference

#include <mag3110.h>

Collaboration diagram for MAG3110_DR_STATUS_t:
Collaboration graph

Data Fields

struct {
   uint8_t   xdr: 1
 
   uint8_t   ydr: 1
 
   uint8_t   zdr: 1
 
   uint8_t   zyxdr: 1
 
   uint8_t   xow: 1
 
   uint8_t   yow: 1
 
   uint8_t   zow: 1
 
   uint8_t   zyxow: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 47 of file mag3110.h.

Field Documentation

◆ b

struct { ... } b

◆ w

uint8_t w

Definition at line 66 of file mag3110.h.

◆ xdr

uint8_t xdr

Definition at line 49 of file mag3110.h.

◆ xow

uint8_t xow

Definition at line 57 of file mag3110.h.

◆ ydr

uint8_t ydr

Definition at line 51 of file mag3110.h.

◆ yow

uint8_t yow

Definition at line 59 of file mag3110.h.

◆ zdr

uint8_t zdr

Definition at line 53 of file mag3110.h.

◆ zow

uint8_t zow

Definition at line 61 of file mag3110.h.

◆ zyxdr

uint8_t zyxdr

Definition at line 55 of file mag3110.h.

◆ zyxow

uint8_t zyxow

Definition at line 63 of file mag3110.h.


The documentation for this union was generated from the following file: