ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
MAG3110_SYSMOD_t Union Reference

#include <mag3110.h>

Collaboration diagram for MAG3110_SYSMOD_t:
Collaboration graph

Data Fields

struct {
   uint8_t   sysmod: 2
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 215 of file mag3110.h.

Field Documentation

◆ b

struct { ... } b

◆ sysmod

uint8_t sysmod

Definition at line 217 of file mag3110.h.

◆ w

uint8_t w

Definition at line 220 of file mag3110.h.


The documentation for this union was generated from the following file: