ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
MAG3110_OFF_X_LSB_t Union Reference

#include <mag3110.h>

Collaboration diagram for MAG3110_OFF_X_LSB_t:
Collaboration graph

Data Fields

struct {
   uint8_t   _reserved_: 1
 
   uint8_t   off_x_lsb: 7
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 258 of file mag3110.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 260 of file mag3110.h.

◆ b

struct { ... } b

◆ off_x_lsb

uint8_t off_x_lsb

Definition at line 261 of file mag3110.h.

◆ w

uint8_t w

Definition at line 264 of file mag3110.h.


The documentation for this union was generated from the following file: