ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
MAG3110_OFF_Z_LSB_t Union Reference

#include <mag3110.h>

Collaboration diagram for MAG3110_OFF_Z_LSB_t:
Collaboration graph

Data Fields

struct {
   uint8_t   _reserved_: 1
 
   uint8_t   off_z_lsb: 7
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 332 of file mag3110.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 334 of file mag3110.h.

◆ b

struct { ... } b

◆ off_z_lsb

uint8_t off_z_lsb

Definition at line 335 of file mag3110.h.

◆ w

uint8_t w

Definition at line 338 of file mag3110.h.


The documentation for this union was generated from the following file: