ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
MAG3110_CTRL_REG1_t Union Reference

#include <mag3110.h>

Collaboration diagram for MAG3110_CTRL_REG1_t:
Collaboration graph

Data Fields

struct {
   uint8_t   ac: 1
 
   uint8_t   tm: 1
 
   uint8_t   fr: 1
 
   uint8_t   os: 2
 
   uint8_t   dr: 3
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 371 of file mag3110.h.

Field Documentation

◆ ac

uint8_t ac

Definition at line 373 of file mag3110.h.

◆ b

struct { ... } b

◆ dr

uint8_t dr

Definition at line 382 of file mag3110.h.

◆ fr

uint8_t fr

Definition at line 377 of file mag3110.h.

◆ os

uint8_t os

Definition at line 380 of file mag3110.h.

◆ tm

uint8_t tm

Definition at line 375 of file mag3110.h.

◆ w

uint8_t w

Definition at line 385 of file mag3110.h.


The documentation for this union was generated from the following file: