ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
MAG3110_CTRL_REG2_t Union Reference

#include <mag3110.h>

Collaboration diagram for MAG3110_CTRL_REG2_t:
Collaboration graph

Data Fields

struct {
   uint8_t   _reserved_: 4
 
   uint8_t   mag_rst: 1
 
   uint8_t   raw: 1
 
   uint8_t   _reserved_1: 1
 
   uint8_t   auto_msrt_en: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 440 of file mag3110.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 442 of file mag3110.h.

◆ _reserved_1

uint8_t _reserved_1

Definition at line 447 of file mag3110.h.

◆ auto_msrt_en

uint8_t auto_msrt_en

Definition at line 448 of file mag3110.h.

◆ b

struct { ... } b

◆ mag_rst

uint8_t mag_rst

Definition at line 443 of file mag3110.h.

◆ raw

uint8_t raw

Definition at line 445 of file mag3110.h.

◆ w

uint8_t w

Definition at line 451 of file mag3110.h.


The documentation for this union was generated from the following file: