ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
MMA8491Q_OUT_X_LSB_t Union Reference

#include <mma8491q.h>

Collaboration diagram for MMA8491Q_OUT_X_LSB_t:
Collaboration graph

Data Fields

struct {
   uint8_t   _reserved_: 2
 
   uint8_t   out_x_lsb: 6
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 106 of file mma8491q.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 110 of file mma8491q.h.

◆ b

struct { ... } b

◆ out_x_lsb

uint8_t out_x_lsb

Definition at line 111 of file mma8491q.h.

◆ w

uint8_t w

Definition at line 114 of file mma8491q.h.


The documentation for this union was generated from the following file: